public interface FlatPatternSettings extends TaggedObject
Modifier and Type | Interface and Description |
---|---|
static class |
FlatPatternSettings.FlatPatternCalloutTypeDisplay
The members of the following structure are the display data for a
callout in a flat pattern drawing member view.
|
static class |
FlatPatternSettings.FlatPatternObjectType
The members of the following enumerated type are used to identify
object types to the FlatPatternView API.
|
static class |
FlatPatternSettings.FlatPatternObjectTypeDisplay
The members of the following structure are the display data for an
object in a flat pattern drawing member view.
|
printTestData, printTestData, tag, tagValue
FlatPatternSettings.FlatPatternObjectTypeDisplay getFlatPatternObjectTypeDisplay(FlatPatternSettings.FlatPatternObjectType objectType) throws NXException, RemoteException
objectType
- The object type for which to return the display data.NXException
RemoteException
void setFlatPatternObjectTypeDisplay(FlatPatternSettings.FlatPatternObjectType objectType, FlatPatternSettings.FlatPatternObjectTypeDisplay displayData) throws NXException, RemoteException
objectType
- The object type for which to get the display data.displayData
- The display data for the flat pattern object type.NXException
RemoteException
FlatPatternSettings.FlatPatternCalloutTypeDisplay getFlatPatternCalloutTypeDisplay(String calloutType) throws NXException, RemoteException
FlatPatternSettings.FlatPatternCalloutTypeDisplay
is separately allocated from the callout_type argument string.
In some cases the new string will contain an
extended form of the callout_type passed in, and that form should
be used for subsequent calls, without modification.
calloutType
- The name of the callout type for which to get the display data.NXException
RemoteException
void setFlatPatternCalloutTypeDisplay(String calloutType, FlatPatternSettings.FlatPatternCalloutTypeDisplay displayData) throws NXException, RemoteException
calloutType
- The name of the callout type for which to set the display data.displayData
- The display data for the callout type.NXException
RemoteException
FlatPatternSettings.FlatPatternObjectTypeDisplay[] getFlatPatternAllObjectTypeDisplay() throws NXException, RemoteException
NXException
RemoteException
FlatPatternSettings.FlatPatternCalloutTypeDisplay[] getFlatPatternAllCalloutTypeDisplay() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.