Package | Description |
---|---|
nxopen.shapesearch |
Provides classes and interfaces for Shape Search.
|
Modifier and Type | Field and Description |
---|---|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.P25P400
search with shape size 25%-400% condition
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.P50P200
search with shape size 50%-200% condition
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.P70P130
search with shape size 70%-130% condition
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.P80P120
search with shape size 80%-120% condition
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.P90P110
search with shape size 90%-110% condition
|
Modifier and Type | Method and Description |
---|---|
ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.searchShapeSize()
Returns the shape size to be set for search.
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShapeSearchBuilder.ShapeSize |
ShapeSearchBuilder.ShapeSize.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShapeSearchBuilder.ShapeSize[] |
ShapeSearchBuilder.ShapeSize.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShapeSearchBuilder.setSearchShapeSize(ShapeSearchBuilder.ShapeSize searchShapeSize)
License requirements: shape_search ("Shape Search") . |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.