Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LogicalConnection
Represents a connection between mutiple From and To
Routing.LogicalTerminal . |
Modifier and Type | Interface and Description |
---|---|
interface |
CableConnection
Connection used by a
CableDevice . |
interface |
Connection
The electrical usage of a
LogicalConnection , restricted to
one From and one To terminal. |
interface |
JumperConnection
A jumper connection connects ports on the same connector.
|
interface |
NonPathConnection
Describes a connection that does not have a path
A pathless connection represents the abilitiy for objects to be connected even though there is not an explicit path between them. |
interface |
PathConnection
Describes a connection that has a path
From and To terminals are not coincident and need a path definition to be routable. |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.