public interface StockTransition extends Stock
StockTransition
object. StockTransition
covers C1 continuous ISegment
in between two stocks. It acts as transition from CrossSection
of one Stock
to another.
When two different Stock
are connected with set of segments, then a stockTransition can be used to cover
it in such a way that CrossSection
at each end of this segments matches with the stock at that location.
These segments can be a routing path, or just a collection of segments.
Stock
covers segments, and StockTransition
inherits
that behavior. However, StockTransition
refers to two end Stock
and the CrossSection
of StockTransition
object varies from one end to another. Stock.PortsData
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
addSegments, alignStock, colorBodies, enableFeatures, getAnchor, getComponent, getCrossSection, getFeatures, getFlippedStatus, getNameStatus, getOriginalLength, getPorts, getProfileEnd, getRotationAngle, getSegments, getStockData, getStockStyle, getStockUse, getTwistAngle, negateOffsetsFlag, removeSegments, renameStockComponent, setAnchor, setCrossSection, setFlippedStatus, setNegateOffsetsFlag, setProfileEnd, setRotationAngle, setStockData, setStockStyle, setTwistAngle, syncComponentAttrs
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
deleteCharacterstics, getCharacteristics, getDestinationCharacteristics, getIntegerCharacteristic, getRealCharacteristic, getStringCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic2, setCharacteristic2, setCharacteristic2, setCharacteristics, setCharacteristics2
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.