public static class SplinePathBuilder.SplinePathAttributeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_RADIUS
A radius method option for spline user attribute
|
static int |
_RATIO_TO_DIAMETER
A ratio to diameter method option for spline user attribute
|
static SplinePathBuilder.SplinePathAttributeOptions |
RADIUS
A radius method option for spline user attribute
|
static SplinePathBuilder.SplinePathAttributeOptions |
RATIO_TO_DIAMETER
A ratio to diameter method option for spline user attribute
|
Modifier and Type | Method and Description |
---|---|
static SplinePathBuilder.SplinePathAttributeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.SplinePathAttributeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.SplinePathAttributeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final SplinePathBuilder.SplinePathAttributeOptions RADIUS
public static final SplinePathBuilder.SplinePathAttributeOptions RATIO_TO_DIAMETER
public static final int _RADIUS
public static final int _RATIO_TO_DIAMETER
public static SplinePathBuilder.SplinePathAttributeOptions valueOf(int value)
public static SplinePathBuilder.SplinePathAttributeOptions valueOf(String name)
public static SplinePathBuilder.SplinePathAttributeOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.