public interface RoutingSystem extends NXObject
Run
objects. RoutingSystem
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
void |
addRuns(Run[] runs)
Adds
Run objects to a RoutingSystem
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX4.0.0 |
String |
getId()
Returns name of routing.
|
Run[] |
getRuns()
Retrieves all
Run objects in RoutingSystem
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX4.0.0 |
void |
removeRuns(Run[] runs)
Removes
Run objects from a RoutingSystem. |
void |
setId(String name)
Sets name of routing.
|
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
String getId() throws NXException, RemoteException
NXException
RemoteException
void setId(String name) throws NXException, RemoteException
name
- Name given to routingNXException
RemoteException
Run[] getRuns() throws NXException, RemoteException
Run
objects in RoutingSystem
NXException
RemoteException
void addRuns(Run[] runs) throws NXException, RemoteException
Run
objects to a RoutingSystem
runs
- Runs to add to the RoutingSytemNXException
RemoteException
void removeRuns(Run[] runs) throws NXException, RemoteException
Run
objects from a RoutingSystem. Only removes
Run from the RoutingSystem, does not remove the Run definition
runs
- Runs to remove from the RoutingSytemNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.