public static class DeviceRelationship.RelationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ASSOCIATED_EQUIPMENT
the related single devices are attached to the relating single device
|
static DeviceRelationship.RelationType |
ASSOCIATED_EQUIPMENT
the related single devices are attached to the relating single device
|
Modifier and Type | Method and Description |
---|---|
static DeviceRelationship.RelationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeviceRelationship.RelationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeviceRelationship.RelationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DeviceRelationship.RelationType ASSOCIATED_EQUIPMENT
public static final int _ASSOCIATED_EQUIPMENT
public static DeviceRelationship.RelationType valueOf(int value)
public static DeviceRelationship.RelationType valueOf(String name)
public static DeviceRelationship.RelationType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.