public interface AddFontBuilder extends Builder
AddFontBuilder
Modifier and Type | Method and Description |
---|---|
void |
setBuilderData(Line selLine,
double[] lineCoords,
String fontName,
double fontScale,
int fontLayer)
Takes selected line and information on the font selected which will be used to build the font
License requirements: routing_base ("Routing Basic") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void setBuilderData(Line selLine, double[] lineCoords, String fontName, double fontScale, int fontLayer) throws NXException, RemoteException
selLine
- lineCoords
- Line Coordinates for font element lines.
formatted as x11,y11,x12,y12,x21,y21,x22,y22,x31,...
where first subscript = line number; second subscript = start pt(1) or end pt(2)
example: y32 = y coordinate of the third line's end pointfontName
- Font style chosen, eg "dashed"fontScale
- Length dimension of font element measured along selected line; font element length = 2.0 * fontScalefontLayer
- 1,2,..255 are valid layers; -1 indicates font to be created in same layer as selLineNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.