public static class SessionVisualizationHighQualityImage.ImageSizeType extends Enum
Modifier and Type | Method and Description |
---|---|
static SessionVisualizationHighQualityImage.ImageSizeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionVisualizationHighQualityImage.ImageSizeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionVisualizationHighQualityImage.ImageSizeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionVisualizationHighQualityImage.ImageSizeType FILL_VIEW
public static final SessionVisualizationHighQualityImage.ImageSizeType ANSI_A
public static final SessionVisualizationHighQualityImage.ImageSizeType ANSI_B
public static final SessionVisualizationHighQualityImage.ImageSizeType ANSI_C
public static final SessionVisualizationHighQualityImage.ImageSizeType ANSI_D
public static final SessionVisualizationHighQualityImage.ImageSizeType ANSI_E
public static final SessionVisualizationHighQualityImage.ImageSizeType ISO_A4
public static final SessionVisualizationHighQualityImage.ImageSizeType ISO_A3
public static final SessionVisualizationHighQualityImage.ImageSizeType ISO_A2
public static final SessionVisualizationHighQualityImage.ImageSizeType ISO_A1
public static final SessionVisualizationHighQualityImage.ImageSizeType ISO_A0
public static final SessionVisualizationHighQualityImage.ImageSizeType USER_DEFINED
public static final SessionVisualizationHighQualityImage.ImageSizeType TRUE_SIZE
public static final int _FILL_VIEW
public static final int _ANSI_A
public static final int _ANSI_B
public static final int _ANSI_C
public static final int _ANSI_D
public static final int _ANSI_E
public static final int _ISO_A4
public static final int _ISO_A3
public static final int _ISO_A2
public static final int _ISO_A1
public static final int _ISO_A0
public static final int _USER_DEFINED
public static final int _TRUE_SIZE
public static SessionVisualizationHighQualityImage.ImageSizeType valueOf(int value)
public static SessionVisualizationHighQualityImage.ImageSizeType valueOf(String name)
public static SessionVisualizationHighQualityImage.ImageSizeType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.