public static class SessionSketch.OriginType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INFER_FROM_PLANE_SELECTION
Sketch origin is inferred from placement face
|
static int |
_PROJECT_WORK_PART_ORIGIN
Sketch origin is the projection of the work part origin
|
static SessionSketch.OriginType |
INFER_FROM_PLANE_SELECTION
Sketch origin is inferred from placement face
|
static SessionSketch.OriginType |
PROJECT_WORK_PART_ORIGIN
Sketch origin is the projection of the work part origin
|
Modifier and Type | Method and Description |
---|---|
static SessionSketch.OriginType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionSketch.OriginType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionSketch.OriginType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionSketch.OriginType INFER_FROM_PLANE_SELECTION
public static final SessionSketch.OriginType PROJECT_WORK_PART_ORIGIN
public static final int _INFER_FROM_PLANE_SELECTION
public static final int _PROJECT_WORK_PART_ORIGIN
public static SessionSketch.OriginType valueOf(int value)
public static SessionSketch.OriginType valueOf(String name)
public static SessionSketch.OriginType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.