public static class SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PARENT_OBJECT
Indicates that display of linked and extracted geometry properties inherits from parent object
|
static int |
_PART_DEFAULT
Indicates that display of linked and extracted geometry properties inherits from part default
|
static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance |
PARENT_OBJECT
Indicates that display of linked and extracted geometry properties inherits from parent object
|
static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance |
PART_DEFAULT
Indicates that display of linked and extracted geometry properties inherits from part default
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance PARENT_OBJECT
public static final SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance PART_DEFAULT
public static final int _PARENT_OBJECT
public static final int _PART_DEFAULT
public static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance valueOf(int value)
public static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance valueOf(String name)
public static SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.