public class ReferenceSetBehavior extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Inherit all PMI regardless of whether the referenced objects are in the active reference set.
|
static int |
_NONE
No PMI will be inherited if any of the PMI objects has a reference to an object which is not in the active reference set.
|
static int |
_PARTIAL
Inherit only PMI for which all of the referenced objects are in the active reference set.
|
static ReferenceSetBehavior |
ALL
Inherit all PMI regardless of whether the referenced objects are in the active reference set.
|
static ReferenceSetBehavior |
NONE
No PMI will be inherited if any of the PMI objects has a reference to an object which is not in the active reference set.
|
static ReferenceSetBehavior |
PARTIAL
Inherit only PMI for which all of the referenced objects are in the active reference set.
|
Modifier and Type | Method and Description |
---|---|
static ReferenceSetBehavior |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReferenceSetBehavior |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReferenceSetBehavior[] |
values()
Returns an array that contains the values for this enum.
|
public static final ReferenceSetBehavior NONE
public static final ReferenceSetBehavior PARTIAL
public static final ReferenceSetBehavior ALL
public static final int _NONE
public static final int _PARTIAL
public static final int _ALL
public static ReferenceSetBehavior valueOf(int value)
public static ReferenceSetBehavior valueOf(String name)
public static ReferenceSetBehavior[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.