public static class PartVisualizationShade.ShadedViewToleranceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_COARSE
For Coarse: Facet Edge Tolerance is 0.01, Facet
Chord Tolerance is 0.01, and Angular Tolerance is 0.0
|
static int |
_CUSTOMIZE
Customize.
|
static int |
_EXTRAFINE
For Extrafine: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.001, and Angular Tolerance is 6
|
static int |
_FINE
For Fine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0025, and Angular Tolerance is 6
|
static int |
_STANDARD
For Standard: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.005 , and Angular Tolerance is 15
|
static int |
_ULTRAFINE
For Ultrafine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0005, and Angular Tolerance is 3
|
static PartVisualizationShade.ShadedViewToleranceType |
COARSE
For Coarse: Facet Edge Tolerance is 0.01, Facet
Chord Tolerance is 0.01, and Angular Tolerance is 0.0
|
static PartVisualizationShade.ShadedViewToleranceType |
CUSTOMIZE
Customize.
|
static PartVisualizationShade.ShadedViewToleranceType |
EXTRAFINE
For Extrafine: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.001, and Angular Tolerance is 6
|
static PartVisualizationShade.ShadedViewToleranceType |
FINE
For Fine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0025, and Angular Tolerance is 6
|
static PartVisualizationShade.ShadedViewToleranceType |
STANDARD
For Standard: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.005 , and Angular Tolerance is 15
|
static PartVisualizationShade.ShadedViewToleranceType |
ULTRAFINE
For Ultrafine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0005, and Angular Tolerance is 3
|
Modifier and Type | Method and Description |
---|---|
static PartVisualizationShade.ShadedViewToleranceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationShade.ShadedViewToleranceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationShade.ShadedViewToleranceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartVisualizationShade.ShadedViewToleranceType COARSE
public static final PartVisualizationShade.ShadedViewToleranceType STANDARD
public static final PartVisualizationShade.ShadedViewToleranceType FINE
public static final PartVisualizationShade.ShadedViewToleranceType EXTRAFINE
public static final PartVisualizationShade.ShadedViewToleranceType ULTRAFINE
public static final PartVisualizationShade.ShadedViewToleranceType CUSTOMIZE
public static final int _COARSE
public static final int _STANDARD
public static final int _FINE
public static final int _EXTRAFINE
public static final int _ULTRAFINE
public static final int _CUSTOMIZE
public static PartVisualizationShade.ShadedViewToleranceType valueOf(int value)
public static PartVisualizationShade.ShadedViewToleranceType valueOf(String name)
public static PartVisualizationShade.ShadedViewToleranceType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.