public static class PartVisualizationShade.HiddenShadedFaceEdges extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DASHED
If selected, hidden shaded face edges are
displayed in the body color with a dashed line
font.
|
static int |
_HIDDEN_COLOR
If any color is selected, hidden shaded face
edges are displayed in that color.
|
static int |
_INVISIBLE
If selected, shaded face edges that are
hidden are not displayed
|
static PartVisualizationShade.HiddenShadedFaceEdges |
DASHED
If selected, hidden shaded face edges are
displayed in the body color with a dashed line
font.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
HIDDEN_COLOR
If any color is selected, hidden shaded face
edges are displayed in that color.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
INVISIBLE
If selected, shaded face edges that are
hidden are not displayed
|
Modifier and Type | Method and Description |
---|---|
static PartVisualizationShade.HiddenShadedFaceEdges |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationShade.HiddenShadedFaceEdges[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartVisualizationShade.HiddenShadedFaceEdges INVISIBLE
public static final PartVisualizationShade.HiddenShadedFaceEdges DASHED
public static final PartVisualizationShade.HiddenShadedFaceEdges HIDDEN_COLOR
public static final int _INVISIBLE
public static final int _DASHED
public static final int _HIDDEN_COLOR
public static PartVisualizationShade.HiddenShadedFaceEdges valueOf(int value)
public static PartVisualizationShade.HiddenShadedFaceEdges valueOf(String name)
public static PartVisualizationShade.HiddenShadedFaceEdges[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.