Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Class and Description |
---|
DisplayedConstraintCollection
a collection of displayed constraints
To obtain an instance of this class, refer to Part Created in NX7.5.0 |
Class and Description |
---|
ComponentConstraint
Constraint for use in positioning assembly objects in NX.
|
ComponentConstraintGroup
Constraint group which represents a group of component constraints in NX.
|
ComponentConstraintGroupBuilder
Represents a
ComponentConstraintGroupBuilder builder To create a new instance of this class, use ComponentAssembly.createConstraintGroupBuilder(nxopen.positioning.ComponentConstraintGroup, nxopen.assemblies.Component) Default values. |
ComponentPositioner
An instance of this class can be used to create
Constraint s and
associated objects. |
MatingConverter
An instance of this class can be used to convert Mating Conditions
to Assembly Constraints in its owning assembly or in child parts
of its owning assembly.
|
Class and Description |
---|
ComponentConstraint
Constraint for use in positioning assembly objects in NX.
|
Class and Description |
---|
Constraint
Constraint for use in positioning objects in NX.
|
Class and Description |
---|
ComponentConstraint
Constraint for use in positioning assembly objects in NX.
|
ComponentConstraint.DirectionToFixed
Specifies how a constraint affects the positioning of a component.
|
ComponentConstraintGroup.ConstraintsCollectionType
the enum to define constraint collection type
|
ComponentNetwork.ArrangementsMode
Specifies how changes in the network are applied to arrangements.
|
Constraint
Constraint for use in positioning objects in NX.
|
Constraint.Alignment
Specifies alignment of directed geometries used in a constraint.
|
Constraint.SolverStatus
Specifies the status of a constraint.
|
Constraint.SplineType
Specifies how the spline points define the shape of the spline.
|
Constraint.Type
Specifies the type of a constraint.
|
ConstraintCollection
a collection of constraints
To obtain an instance of this class, refer to Positioner Created in NX5.0.0 |
ConstraintReference
ConstraintReference for use in positioning objects in NX.
|
ConstraintReference.ConstraintOrder
Specifies the order of the constraint reference used in a
Constraint . |
ConstraintReference.GeometryType
Specifies the type of the geometry used in a
ConstraintReference . |
ConstraintReference.HalfSpace
Specifies the half space value of one geometry used in a distance constraint.
|
DisplayedConstraint
The displayed representation of a constraint, used for graphical
display and to represent it in the Assembly Navigator.
|
MatingConverter.PartContext
Defines in which parts mating conditions will be converted.
|
Network
Network for use in positioning objects in NX.
|
Network.ObjectStatus
Specifies the solver status of a movable object.
|
Positioner
An instance of this class can be used to create
Constraint s and
associated objects. |
Class and Description |
---|
Constraint
Constraint for use in positioning objects in NX.
|
Constraint.SplineType
Specifies how the spline points define the shape of the spline.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.