public static class ConstraintReference.GeometryType extends Enum
ConstraintReference
.
The type reflects that used in a Constraint
while it is being
solved and may be different from that inferred directly from
ConstraintReference.getGeometry()
. For example we may use
LINE
as an axis when given a cylindrical face as the geometry.Modifier and Type | Method and Description |
---|---|
static ConstraintReference.GeometryType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConstraintReference.GeometryType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConstraintReference.GeometryType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ConstraintReference.GeometryType UNKNOWN
public static final ConstraintReference.GeometryType POINT
public static final ConstraintReference.GeometryType LINE
public static final ConstraintReference.GeometryType CIRCLE
public static final ConstraintReference.GeometryType PLANE
public static final ConstraintReference.GeometryType CYLINDER
public static final ConstraintReference.GeometryType SPHERE
public static final ConstraintReference.GeometryType SWEEP_SURFACE
public static final ConstraintReference.GeometryType PARAMETRIC_SURFACE
public static final ConstraintReference.GeometryType PARAMETRIC_CURVE
public static final ConstraintReference.GeometryType SPLINE_CURVE
public static final ConstraintReference.GeometryType TORUS
public static final ConstraintReference.GeometryType CONE
public static final ConstraintReference.GeometryType ELLIPSE
public static final ConstraintReference.GeometryType SPLINE_SURFACE
public static final ConstraintReference.GeometryType COORDINATE_SYSTEM
public static final int _UNKNOWN
public static final int _POINT
public static final int _LINE
public static final int _CIRCLE
public static final int _PLANE
public static final int _CYLINDER
public static final int _SPHERE
public static final int _SWEEP_SURFACE
public static final int _PARAMETRIC_SURFACE
public static final int _PARAMETRIC_CURVE
public static final int _SPLINE_CURVE
public static final int _TORUS
public static final int _CONE
public static final int _ELLIPSE
public static final int _SPLINE_SURFACE
public static final int _COORDINATE_SYSTEM
public static ConstraintReference.GeometryType valueOf(int value)
public static ConstraintReference.GeometryType valueOf(String name)
public static ConstraintReference.GeometryType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.