public interface PartOperationValidationPropertiesBuilder extends AttributePropertiesBuilder
PartOperationValidationPropertiesBuilder
to be used
for overriding the default validation parameters for a part in import operation.
PdmSession.createPartOperationValidationPropertiesBuilder(nxopen.NXObject[])
Property | Value |
---|---|
BooleanValue | False |
DataType | String |
IntegerValue | 0 |
NumberValue | 0 |
ObjectPicker (deprecated) | Object |
AttributePropertiesBuilder.OperationType
AttributePropertiesBaseBuilder.BooleanValueOptions, AttributePropertiesBaseBuilder.DataTypeOptions, AttributePropertiesBaseBuilder.ObjectOptions
Modifier and Type | Method and Description |
---|---|
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
getValidationRuleSetBrowseOption()
Gets the validation rule set browse option
License requirements: None. |
String |
getValidationRuleSetFile()
Gets the validation rule set file
License requirements: None. |
boolean |
getValidationTreatOutdatedAsPass()
Gets the validation treat outdated as pass flag
License requirements: None. |
boolean |
getValidationTreatWarningAsPass()
Gets the validation treat warning as pass flag
License requirements: None. |
void |
setValidationRuleSetBrowseOption(PartOperationImportBuilder.ValidationRuleSetFileBrowseOption validationRuleSetBrowseOption)
Sets the validation rule set browse option
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
setValidationRuleSetFile(String filename)
Sets the validation rule set file
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
setValidationTreatOutdatedAsPass(boolean validationTreatOutdatedAsPass)
Sets the validation treat outdated as pass flag
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
setValidationTreatWarningAsPass(boolean validationTreatWarningAsPass)
Sets the validation treat warning as pass flag
License requirements: assemblies ("ASSEMBLIES MODULE") . |
applyUnits, arrayIndex, booleanValue, category, createAttribute, dataType, dateValue, delete, deleteArray, expression, integerValue, isArray, isReferenceType, lockOnSave, numberValue, objectPicker, selectedObjects, setArray, setArrayIndex, setAttributeObjects, setBooleanValue, setCategory, setDataType, setExpression, setIntegerValue, setLockOnSave, setNumberValue, setObjectPicker, setReferenceType, setStringValue, setTitle, setUnits, setValueAlias, stringValue, title, units, valueAlias
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption getValidationRuleSetBrowseOption() throws NXException, RemoteException
NXException
RemoteException
void setValidationRuleSetBrowseOption(PartOperationImportBuilder.ValidationRuleSetFileBrowseOption validationRuleSetBrowseOption) throws NXException, RemoteException
validationRuleSetBrowseOption
- NXException
RemoteException
String getValidationRuleSetFile() throws NXException, RemoteException
NXException
RemoteException
void setValidationRuleSetFile(String filename) throws NXException, RemoteException
filename
- NXException
RemoteException
boolean getValidationTreatWarningAsPass() throws NXException, RemoteException
NXException
RemoteException
void setValidationTreatWarningAsPass(boolean validationTreatWarningAsPass) throws NXException, RemoteException
validationTreatWarningAsPass
- NXException
RemoteException
boolean getValidationTreatOutdatedAsPass() throws NXException, RemoteException
NXException
RemoteException
void setValidationTreatOutdatedAsPass(boolean validationTreatOutdatedAsPass) throws NXException, RemoteException
validationTreatOutdatedAsPass
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.