public static class PartOperationImportBuilder.Validation extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT |
static int |
_IMPORT_FROM_PART |
static int |
_OFF |
static int |
_RUN_VALIDATION |
static int |
_RUN_VALIDATION_HYBRID |
static PartOperationImportBuilder.Validation |
DEFAULT |
static PartOperationImportBuilder.Validation |
IMPORT_FROM_PART |
static PartOperationImportBuilder.Validation |
OFF |
static PartOperationImportBuilder.Validation |
RUN_VALIDATION |
static PartOperationImportBuilder.Validation |
RUN_VALIDATION_HYBRID |
Modifier and Type | Method and Description |
---|---|
static PartOperationImportBuilder.Validation |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartOperationImportBuilder.Validation |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartOperationImportBuilder.Validation[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartOperationImportBuilder.Validation OFF
public static final PartOperationImportBuilder.Validation IMPORT_FROM_PART
public static final PartOperationImportBuilder.Validation RUN_VALIDATION
public static final PartOperationImportBuilder.Validation RUN_VALIDATION_HYBRID
public static final PartOperationImportBuilder.Validation DEFAULT
public static final int _OFF
public static final int _IMPORT_FROM_PART
public static final int _RUN_VALIDATION
public static final int _RUN_VALIDATION_HYBRID
public static final int _DEFAULT
public static PartOperationImportBuilder.Validation valueOf(int value)
public static PartOperationImportBuilder.Validation valueOf(String name)
public static PartOperationImportBuilder.Validation[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.