public static class PostProcess.EnvelopeTolerance extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
PostProcess.EnvelopeAccuracyModes |
accuracyMode
Accuracy mode.
|
boolean |
decimationEnabled
Indicates if decimation is enabled or not.
|
double |
decimationFactor
Specifies targeted decimation rate which is decimated body/original body.
|
double |
decimationMaxError
Specifies max decimation error: (bigger than 0): percentage, (less than 0): absolute value.
|
double |
tolerance
Tolerance value.
|
PostProcess.EnvelopeToleranceTypes |
toleranceType
Indicates if envelopeTolerance is specified as percentage value or absolute value.
|
Constructor and Description |
---|
EnvelopeTolerance() |
EnvelopeTolerance(PostProcess.EnvelopeAccuracyModes accuracyModeInitial,
PostProcess.EnvelopeToleranceTypes toleranceTypeInitial,
double toleranceInitial,
boolean decimationEnabledInitial,
double decimationFactorInitial,
double decimationMaxErrorInitial)
Constructor for the EnvelopeTolerance object.
|
public PostProcess.EnvelopeAccuracyModes accuracyMode
Motion.PostProcess.EnvelopeAccuracyModes
.public PostProcess.EnvelopeToleranceTypes toleranceType
Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.public double tolerance
Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.public boolean decimationEnabled
Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.public double decimationFactor
Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.public double decimationMaxError
Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.public EnvelopeTolerance()
public EnvelopeTolerance(PostProcess.EnvelopeAccuracyModes accuracyModeInitial, PostProcess.EnvelopeToleranceTypes toleranceTypeInitial, double toleranceInitial, boolean decimationEnabledInitial, double decimationFactorInitial, double decimationMaxErrorInitial)
accuracyModeInitial
- Accuracy mode. Motion.PostProcess.EnvelopeAccuracyModes
.toleranceTypeInitial
- Indicates if envelopeTolerance is specified as percentage value or absolute value. Used only if accurcayMode is Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.toleranceInitial
- Tolerance value. Used only if accurcayMode is Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.decimationEnabledInitial
- Indicates if decimation is enabled or not. Used only if accurcayMode is Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.decimationFactorInitial
- Specifies targeted decimation rate which is decimated body/original body. Used only if accurcayMode is Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.decimationMaxErrorInitial
- Specifies max decimation error: (bigger than 0): percentage, (less than 0): absolute value. Used only if accurcayMode is Motion.PostProcess.EnvelopeAccuracyModes#CUSTOM
.Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.