public static class PackagingMeasureBuilder.MeasureType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANGLE
Measure angle between lines or linear edges.
|
static int |
_MINIMUM_DISTANCE
Measure minimum distance between objects.
|
static PackagingMeasureBuilder.MeasureType |
ANGLE
Measure angle between lines or linear edges.
|
static PackagingMeasureBuilder.MeasureType |
MINIMUM_DISTANCE
Measure minimum distance between objects.
|
Modifier and Type | Method and Description |
---|---|
static PackagingMeasureBuilder.MeasureType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingMeasureBuilder.MeasureType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingMeasureBuilder.MeasureType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PackagingMeasureBuilder.MeasureType MINIMUM_DISTANCE
public static final PackagingMeasureBuilder.MeasureType ANGLE
public static final int _MINIMUM_DISTANCE
public static final int _ANGLE
public static PackagingMeasureBuilder.MeasureType valueOf(int value)
public static PackagingMeasureBuilder.MeasureType valueOf(String name)
public static PackagingMeasureBuilder.MeasureType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.