public interface MotionSolutionCollection extends TaggedObjectCollection
MotionManager
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
MotionSolutionBuilder |
createSolutionBuilder(MotionSolution solution)
Creates an
MotionSolutionBuilder . |
void |
deleteSolution(MotionSolution tSolution,
boolean ifDeleteResult)
Delete the
MotionSolution object of current session. |
MotionSolution |
findObject(String name)
Finds the
MotionSolution object with the given name. |
MotionSolution |
getActiveSolution()
Get the active
MotionSolution object of current session. |
void |
setActiveSolution(MotionSolution activeSolution)
Set the active
MotionSolution object of current session. |
_find_next, iterator
MotionSolutionBuilder createSolutionBuilder(MotionSolution solution) throws NXException, RemoteException
MotionSolutionBuilder
. This class
is used to construct an MotionSolution
object.
solution
- "MotionSolution
to be edited,
if null then create a new oneNXException
RemoteException
MotionSolution findObject(String name) throws NXException, RemoteException
MotionSolution
object with the given name.
An exception will be thrown if no object can be found with given name.
name
- Name of the Solution object.MotionSolution
object with this name.NXException
RemoteException
MotionSolution getActiveSolution() throws NXException, RemoteException
MotionSolution
object of current session.
MotionSolution
NXException
RemoteException
void setActiveSolution(MotionSolution activeSolution) throws NXException, RemoteException
MotionSolution
object of current session.
activeSolution
- the active solution MotionSolution
NXException
RemoteException
void deleteSolution(MotionSolution tSolution, boolean ifDeleteResult) throws NXException, RemoteException
MotionSolution
object of current session.
tSolution
- the MotionSolution
object to be deletedifDeleteResult
- Delete the result files if it is trueNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.