public static class GeneralCouplerBuilder.AttachmentType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_THREE
three-joint coupler type
|
static int |
_TWO
two-joint coupler type
|
static GeneralCouplerBuilder.AttachmentType |
THREE
three-joint coupler type
|
static GeneralCouplerBuilder.AttachmentType |
TWO
two-joint coupler type
|
Modifier and Type | Method and Description |
---|---|
static GeneralCouplerBuilder.AttachmentType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralCouplerBuilder.AttachmentType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralCouplerBuilder.AttachmentType[] |
values()
Returns an array that contains the values for this enum.
|
public static final GeneralCouplerBuilder.AttachmentType TWO
public static final GeneralCouplerBuilder.AttachmentType THREE
public static final int _TWO
public static final int _THREE
public static GeneralCouplerBuilder.AttachmentType valueOf(int value)
public static GeneralCouplerBuilder.AttachmentType valueOf(String name)
public static GeneralCouplerBuilder.AttachmentType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.