public static class ConnectorBuilder.AttachmentType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LINK
connector is attacted to links
|
static int |
_REVOLUTE_JOINT
connector is attacted to revolute joint
|
static int |
_SLIDER_JOINT
connector is attacted to slider joint
|
static ConnectorBuilder.AttachmentType |
LINK
connector is attacted to links
|
static ConnectorBuilder.AttachmentType |
REVOLUTE_JOINT
connector is attacted to revolute joint
|
static ConnectorBuilder.AttachmentType |
SLIDER_JOINT
connector is attacted to slider joint
|
Modifier and Type | Method and Description |
---|---|
static ConnectorBuilder.AttachmentType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConnectorBuilder.AttachmentType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConnectorBuilder.AttachmentType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ConnectorBuilder.AttachmentType LINK
public static final ConnectorBuilder.AttachmentType SLIDER_JOINT
public static final ConnectorBuilder.AttachmentType REVOLUTE_JOINT
public static final int _LINK
public static final int _SLIDER_JOINT
public static final int _REVOLUTE_JOINT
public static ConnectorBuilder.AttachmentType valueOf(int value)
public static ConnectorBuilder.AttachmentType valueOf(String name)
public static ConnectorBuilder.AttachmentType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.