Interface | Description |
---|---|
ContextMenu |
Represents a Context Menu .
|
ContextMenuEntry |
Represents an entry on a context menu.
|
ContextMenuProperties |
Provides information about the MenuBar.ContextMenu object being customized.
|
MenuBarManager |
Interface for the MenuBarManager object
To obtain an instance of this class, refer to UI Created in NX6.0.0 |
MenuBarManager.ActionCallback |
Prototype for the action callbacks
|
MenuBarManager.ConfigureContextMenu |
Prototype for the callback used to configure a context menu.
|
MenuBarManager.EnterMenuApplication |
Prototype for callback called whenever the application is entered
|
MenuBarManager.ExitMenuApplication |
Prototype for callback called whenever the application is exited
|
MenuBarManager.InitializeMenuApplication |
Prototype for application initialization callback
|
MenuButton |
Implements the Object for Menu Buttons .
|
MenuButtonEvent |
Implements the Event Object for Menu Buttons .
|
Class | Description |
---|---|
ContextMenuEntry.Type |
Specifies the type of the menu entry.
|
MenuBarManager.CallbackStatus |
Return values for action callbacks
|
MenuButton.SensitivityStatus |
Sensitivity Status
|
MenuButton.Toggle |
Toggle Status
|
MenuButton.Type |
Available button types
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.