Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
MATLABSignalConnectionBuilder |
MATLABSignalConnectionCollection.createSignalConnectionBuilder(MATLABSignalConnection connection)
Creates a
MATLABSignalConnectionBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX11.0.0 |
MATLABSignalConnectionBuilder |
MATLABSignalConnectionBuilderList.findItem(int index)
Returns the object at the input index.
|
MATLABSignalConnectionBuilder[] |
MATLABSignalConnectionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MATLABSignalConnectionBuilderList.append(MATLABSignalConnectionBuilder object)
Appends an object to the list
License requirements: None. |
void |
MATLABSignalConnectionBuilderList.append(MATLABSignalConnectionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
MATLABSignalConnectionBuilderList.erase(MATLABSignalConnectionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
MATLABSignalConnectionBuilderList.erase(MATLABSignalConnectionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
MATLABSignalConnectionBuilderList.findIndex(MATLABSignalConnectionBuilder obj)
Finds the index where the input object appears.
|
void |
MATLABSignalConnectionBuilderList.insert(int location,
MATLABSignalConnectionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
MATLABSignalConnectionBuilderList.setContents(MATLABSignalConnectionBuilder[] objects)
Sets the contents of the entire list.
|
void |
MATLABSignalConnectionBuilderList.swap(MATLABSignalConnectionBuilder object1,
MATLABSignalConnectionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.