public static class SignalBuilder.IOType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INPUT
Input
|
static int |
_OUTPUT
Output
|
static SignalBuilder.IOType |
INPUT
Input
|
static SignalBuilder.IOType |
OUTPUT
Output
|
Modifier and Type | Method and Description |
---|---|
static SignalBuilder.IOType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalBuilder.IOType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalBuilder.IOType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SignalBuilder.IOType INPUT
public static final SignalBuilder.IOType OUTPUT
public static final int _INPUT
public static final int _OUTPUT
public static SignalBuilder.IOType valueOf(int value)
public static SignalBuilder.IOType valueOf(String name)
public static SignalBuilder.IOType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.