Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.markup |
Provides classes and interfaces relating to Markup.
|
Class and Description |
---|
MarkupManager
Contains the collection objects for creating and iterating over markup objects.
|
Class and Description |
---|
Circle
Represents a
Circle
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createCircle Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Circle.CenterAndRadiusData
This class holds the data returned from
Circle.getCenterAndRadius() |
EditObjectDisplayBuilder
The
EditObjectDisplayBuilder is used to edit display settings of the markup objects. |
Ellipse
Represents a
Ellipse
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createEllipse Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Ellipse.CenterAndRadiusData
This class holds the data returned from
Ellipse.getCenterAndRadius() |
File
Represents a
File
To create a new instance of this class, use nxopen.Markup.MarkupFileCollection#createFile Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Freehand
Represents a
Freehand
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createFreehand Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Icon
Represents a
Icon
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createIcon Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Icon.Size
Represents the possible
Icon size. |
MarkupFileCollection
Represents a
MarkupFileCollection To obtain an instance of this class, refer to MarkupManager Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
MarkupFileObjectCollection |
MarkupObject
Represents a
MarkupObject on the screen. |
MarkupObjectCollection
This collects all the markups in current NX session
To obtain an instance of this class, refer to MarkupManager Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Polyline
Represents a
Polyline
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createPolyline Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Polyline.LineOption
Represents the
Polyline line option. |
Rectangle
Represents a
Rectangle
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createRectangle Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Rectangle.CenterLengthAndWidthData
This class holds the data returned from
Rectangle.getCenterLengthAndWidth() |
Text
Represents a
Text
To create a new instance of this class, use nxopen.Markup.MarkupFileObjectCollection#createText Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.