public static class StepOptionBehavior.StepOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXTEND_NEIGHBORSAT_SMOOTH_EDGE
Extends faces neighboring a smooth edge of the motion face.
|
static int |
_NONE
Does not add step faces.
|
static StepOptionBehavior.StepOptionType |
EXTEND_NEIGHBORSAT_SMOOTH_EDGE
Extends faces neighboring a smooth edge of the motion face.
|
static StepOptionBehavior.StepOptionType |
NONE
Does not add step faces.
|
Modifier and Type | Method and Description |
---|---|
static StepOptionBehavior.StepOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepOptionBehavior.StepOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepOptionBehavior.StepOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final StepOptionBehavior.StepOptionType NONE
public static final StepOptionBehavior.StepOptionType EXTEND_NEIGHBORSAT_SMOOTH_EDGE
public static final int _NONE
public static final int _EXTEND_NEIGHBORSAT_SMOOTH_EDGE
public static StepOptionBehavior.StepOptionType valueOf(int value)
public static StepOptionBehavior.StepOptionType valueOf(String name)
public static StepOptionBehavior.StepOptionType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.