public static class SpiralPattern.SpiralDefineSize extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NUMBER_OF_TURNS
using number of turns to define size of spiral
|
static int |
_TOTAL_ANGLE
using total angle to define size of spiral
|
static SpiralPattern.SpiralDefineSize |
NUMBER_OF_TURNS
using number of turns to define size of spiral
|
static SpiralPattern.SpiralDefineSize |
TOTAL_ANGLE
using total angle to define size of spiral
|
Modifier and Type | Method and Description |
---|---|
static SpiralPattern.SpiralDefineSize |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpiralPattern.SpiralDefineSize |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpiralPattern.SpiralDefineSize[] |
values()
Returns an array that contains the values for this enum.
|
public static final SpiralPattern.SpiralDefineSize NUMBER_OF_TURNS
public static final SpiralPattern.SpiralDefineSize TOTAL_ANGLE
public static final int _NUMBER_OF_TURNS
public static final int _TOTAL_ANGLE
public static SpiralPattern.SpiralDefineSize valueOf(int value)
public static SpiralPattern.SpiralDefineSize valueOf(String name)
public static SpiralPattern.SpiralDefineSize[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.