public static class SimpleDraft.SimpleDraftType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ASYMMETRIC
Draft on both sides of the profile using the not same angle
|
static int |
_MATCHED_ENDS
Draft on both sides of the profile such that the end profiles match in areas
|
static int |
_NO_DRAFT
No draft
|
static int |
_SIMPLE_FROM_PROFILE
Draft using the profile as the reference
|
static int |
_SIMPLE_FROM_START
Draft using the start limit as the reference
|
static int |
_SYMMETRIC
Draft on both sides of the profile using the same angle
|
static SimpleDraft.SimpleDraftType |
ASYMMETRIC
Draft on both sides of the profile using the not same angle
|
static SimpleDraft.SimpleDraftType |
MATCHED_ENDS
Draft on both sides of the profile such that the end profiles match in areas
|
static SimpleDraft.SimpleDraftType |
NO_DRAFT
No draft
|
static SimpleDraft.SimpleDraftType |
SIMPLE_FROM_PROFILE
Draft using the profile as the reference
|
static SimpleDraft.SimpleDraftType |
SIMPLE_FROM_START
Draft using the start limit as the reference
|
static SimpleDraft.SimpleDraftType |
SYMMETRIC
Draft on both sides of the profile using the same angle
|
Modifier and Type | Method and Description |
---|---|
static SimpleDraft.SimpleDraftType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimpleDraft.SimpleDraftType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimpleDraft.SimpleDraftType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimpleDraft.SimpleDraftType NO_DRAFT
public static final SimpleDraft.SimpleDraftType SIMPLE_FROM_START
public static final SimpleDraft.SimpleDraftType SIMPLE_FROM_PROFILE
public static final SimpleDraft.SimpleDraftType SYMMETRIC
public static final SimpleDraft.SimpleDraftType MATCHED_ENDS
public static final SimpleDraft.SimpleDraftType ASYMMETRIC
public static final int _NO_DRAFT
public static final int _SIMPLE_FROM_START
public static final int _SIMPLE_FROM_PROFILE
public static final int _SYMMETRIC
public static final int _MATCHED_ENDS
public static final int _ASYMMETRIC
public static SimpleDraft.SimpleDraftType valueOf(int value)
public static SimpleDraft.SimpleDraftType valueOf(String name)
public static SimpleDraft.SimpleDraftType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.