public static class PatternSpacing.SpacingType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LIST
Specify offsets with a list.
|
static int |
_OFFSET
Specify distance from the origin of one instance to the origin of the next instance.
|
static int |
_PITCH
This is for pattern fill case.
|
static int |
_PITCH_AND_SPAN
Specify distance between instances and distance for all instances, number of copies is calculated.
|
static int |
_POLYGON_COUNT_PER_SIDE
This is for Polygon type.
|
static int |
_POLYGON_PITCH_ALONG_SIDE
This is for Polygon type.
|
static int |
_SPAN
Specify a distance for which all instances should occupy.
|
static PatternSpacing.SpacingType |
LIST
Specify offsets with a list.
|
static PatternSpacing.SpacingType |
OFFSET
Specify distance from the origin of one instance to the origin of the next instance.
|
static PatternSpacing.SpacingType |
PITCH
This is for pattern fill case.
|
static PatternSpacing.SpacingType |
PITCH_AND_SPAN
Specify distance between instances and distance for all instances, number of copies is calculated.
|
static PatternSpacing.SpacingType |
POLYGON_COUNT_PER_SIDE
This is for Polygon type.
|
static PatternSpacing.SpacingType |
POLYGON_PITCH_ALONG_SIDE
This is for Polygon type.
|
static PatternSpacing.SpacingType |
SPAN
Specify a distance for which all instances should occupy.
|
Modifier and Type | Method and Description |
---|---|
static PatternSpacing.SpacingType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternSpacing.SpacingType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternSpacing.SpacingType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PatternSpacing.SpacingType OFFSET
public static final PatternSpacing.SpacingType SPAN
public static final PatternSpacing.SpacingType PITCH_AND_SPAN
public static final PatternSpacing.SpacingType PITCH
public static final PatternSpacing.SpacingType LIST
public static final PatternSpacing.SpacingType POLYGON_COUNT_PER_SIDE
public static final PatternSpacing.SpacingType POLYGON_PITCH_ALONG_SIDE
public static final int _OFFSET
public static final int _SPAN
public static final int _PITCH_AND_SPAN
public static final int _PITCH
public static final int _LIST
public static final int _POLYGON_COUNT_PER_SIDE
public static final int _POLYGON_PITCH_ALONG_SIDE
public static PatternSpacing.SpacingType valueOf(int value)
public static PatternSpacing.SpacingType valueOf(String name)
public static PatternSpacing.SpacingType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.