public static class HighlightLinesAnalysisBuilder.LightPlacements extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BETWEEN_POINTS
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static int |
_THROUGH_POINTS
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static int |
_UNIFORM
Uniform: Lights are placed uniformly on light plane
|
static HighlightLinesAnalysisBuilder.LightPlacements |
BETWEEN_POINTS
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
THROUGH_POINTS
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
UNIFORM
Uniform: Lights are placed uniformly on light plane
|
Modifier and Type | Method and Description |
---|---|
static HighlightLinesAnalysisBuilder.LightPlacements |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HighlightLinesAnalysisBuilder.LightPlacements[] |
values()
Returns an array that contains the values for this enum.
|
public static final HighlightLinesAnalysisBuilder.LightPlacements UNIFORM
public static final HighlightLinesAnalysisBuilder.LightPlacements THROUGH_POINTS
public static final HighlightLinesAnalysisBuilder.LightPlacements BETWEEN_POINTS
public static final int _UNIFORM
public static final int _THROUGH_POINTS
public static final int _BETWEEN_POINTS
public static HighlightLinesAnalysisBuilder.LightPlacements valueOf(int value)
public static HighlightLinesAnalysisBuilder.LightPlacements valueOf(String name)
public static HighlightLinesAnalysisBuilder.LightPlacements[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.