public static class GeometricProperties.OutputType extends Enum
GeometricAnalysis.GeometricProperties.OutputType#DYNAMIC
displays the properties of an entity under the cursor when NX is
run interactively.Modifier and Type | Field and Description |
---|---|
static int |
_DYNAMIC
Properties of an entity are displayed first on the dialog
itself on mouse over.
|
static int |
_STATIC
Propeties of the selected entities are displayed in the
information window.
|
static GeometricProperties.OutputType |
DYNAMIC
Properties of an entity are displayed first on the dialog
itself on mouse over.
|
static GeometricProperties.OutputType |
STATIC
Propeties of the selected entities are displayed in the
information window.
|
Modifier and Type | Method and Description |
---|---|
static GeometricProperties.OutputType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricProperties.OutputType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricProperties.OutputType[] |
values()
Returns an array that contains the values for this enum.
|
public static final GeometricProperties.OutputType DYNAMIC
public static final GeometricProperties.OutputType STATIC
public static final int _DYNAMIC
public static final int _STATIC
public static GeometricProperties.OutputType valueOf(int value)
public static GeometricProperties.OutputType valueOf(String name)
public static GeometricProperties.OutputType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.