Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
BulkHeadListItemBuilder |
BulkHeadsBuilder.createBulkheadListItem(BulkHeadsBuilder.BulkheadType bulkheadsType)
Create a list to generate a single bulkHead.
|
BulkHeadListItemBuilder |
BulkHeadListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
BulkHeadListItemBuilder[] |
BulkHeadListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BulkHeadListItemBuilderList.append(BulkHeadListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
BulkHeadListItemBuilderList.append(BulkHeadListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BulkHeadListItemBuilderList.erase(BulkHeadListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
BulkHeadListItemBuilderList.erase(BulkHeadListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BulkHeadListItemBuilderList.findIndex(BulkHeadListItemBuilder obj)
Finds the index where the input object appears.
|
void |
BulkHeadListItemBuilderList.insert(int location,
BulkHeadListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
BulkHeadListItemBuilderList.setContents(BulkHeadListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
BulkHeadListItemBuilderList.swap(BulkHeadListItemBuilder object1,
BulkHeadListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.