public static class StiffenerBySupportPathBuilder.Method extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGNED_BOUNDARY
Aligned Boundary
|
static int |
_ALIGNED_LENGTH
Aligned Length
|
static int |
_BOUND_TO_BOUND
Bound to Bound
|
static int |
_HORIZONTAL
Horizontal
|
static int |
_NORMAL_TO_CURVE
Normal to Curve
|
static int |
_PARALLEL_TO_LINE
Parallel to Line
|
static int |
_THROUGH_POINT
Through Point
|
static int |
_VERTICAL
Vertical
|
static StiffenerBySupportPathBuilder.Method |
ALIGNED_BOUNDARY
Aligned Boundary
|
static StiffenerBySupportPathBuilder.Method |
ALIGNED_LENGTH
Aligned Length
|
static StiffenerBySupportPathBuilder.Method |
BOUND_TO_BOUND
Bound to Bound
|
static StiffenerBySupportPathBuilder.Method |
HORIZONTAL
Horizontal
|
static StiffenerBySupportPathBuilder.Method |
NORMAL_TO_CURVE
Normal to Curve
|
static StiffenerBySupportPathBuilder.Method |
PARALLEL_TO_LINE
Parallel to Line
|
static StiffenerBySupportPathBuilder.Method |
THROUGH_POINT
Through Point
|
static StiffenerBySupportPathBuilder.Method |
VERTICAL
Vertical
|
Modifier and Type | Method and Description |
---|---|
static StiffenerBySupportPathBuilder.Method |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBySupportPathBuilder.Method |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBySupportPathBuilder.Method[] |
values()
Returns an array that contains the values for this enum.
|
public static final StiffenerBySupportPathBuilder.Method ALIGNED_BOUNDARY
public static final StiffenerBySupportPathBuilder.Method ALIGNED_LENGTH
public static final StiffenerBySupportPathBuilder.Method BOUND_TO_BOUND
public static final StiffenerBySupportPathBuilder.Method PARALLEL_TO_LINE
public static final StiffenerBySupportPathBuilder.Method HORIZONTAL
public static final StiffenerBySupportPathBuilder.Method VERTICAL
public static final StiffenerBySupportPathBuilder.Method NORMAL_TO_CURVE
public static final StiffenerBySupportPathBuilder.Method THROUGH_POINT
public static final int _ALIGNED_BOUNDARY
public static final int _ALIGNED_LENGTH
public static final int _BOUND_TO_BOUND
public static final int _PARALLEL_TO_LINE
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _NORMAL_TO_CURVE
public static final int _THROUGH_POINT
public static StiffenerBySupportPathBuilder.Method valueOf(int value)
public static StiffenerBySupportPathBuilder.Method valueOf(String name)
public static StiffenerBySupportPathBuilder.Method[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.