public static class StiffenerBuilder.EdgeReinforcementPlacementMethods extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ON_EDGE
Attach the edge reinforcement to the edge
|
static int |
_ON_FACE
Attach the edge reinforcement to the adajacent face
|
static StiffenerBuilder.EdgeReinforcementPlacementMethods |
ON_EDGE
Attach the edge reinforcement to the edge
|
static StiffenerBuilder.EdgeReinforcementPlacementMethods |
ON_FACE
Attach the edge reinforcement to the adajacent face
|
Modifier and Type | Method and Description |
---|---|
static StiffenerBuilder.EdgeReinforcementPlacementMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBuilder.EdgeReinforcementPlacementMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBuilder.EdgeReinforcementPlacementMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final StiffenerBuilder.EdgeReinforcementPlacementMethods ON_EDGE
public static final StiffenerBuilder.EdgeReinforcementPlacementMethods ON_FACE
public static final int _ON_EDGE
public static final int _ON_FACE
public static StiffenerBuilder.EdgeReinforcementPlacementMethods valueOf(int value)
public static StiffenerBuilder.EdgeReinforcementPlacementMethods valueOf(String name)
public static StiffenerBuilder.EdgeReinforcementPlacementMethods[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.