public static class ProfileCutoutBuilder.CollarPlateCreationApproaches extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_STEEL_FEATURE
Steel feature approach - User Collar Plate to create collar plate
|
static int |
_TEMPLATE
Template approach - Use Standard Part Framework to create collar plate.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
STEEL_FEATURE
Steel feature approach - User Collar Plate to create collar plate
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
TEMPLATE
Template approach - Use Standard Part Framework to create collar plate.
|
Modifier and Type | Method and Description |
---|---|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches[] |
values()
Returns an array that contains the values for this enum.
|
public static final ProfileCutoutBuilder.CollarPlateCreationApproaches TEMPLATE
public static final ProfileCutoutBuilder.CollarPlateCreationApproaches STEEL_FEATURE
public static final int _TEMPLATE
public static final int _STEEL_FEATURE
public static ProfileCutoutBuilder.CollarPlateCreationApproaches valueOf(int value)
public static ProfileCutoutBuilder.CollarPlateCreationApproaches valueOf(String name)
public static ProfileCutoutBuilder.CollarPlateCreationApproaches[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.