public static class PlateChamferBuilder.AngleMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANGLE
Use the angle for the chamfer parameters
|
static int |
_RATIO
Use the ratio for the chamfer parameters
|
static PlateChamferBuilder.AngleMethod |
ANGLE
Use the angle for the chamfer parameters
|
static PlateChamferBuilder.AngleMethod |
RATIO
Use the ratio for the chamfer parameters
|
Modifier and Type | Method and Description |
---|---|
static PlateChamferBuilder.AngleMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateChamferBuilder.AngleMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateChamferBuilder.AngleMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlateChamferBuilder.AngleMethod ANGLE
public static final PlateChamferBuilder.AngleMethod RATIO
public static final int _ANGLE
public static final int _RATIO
public static PlateChamferBuilder.AngleMethod valueOf(int value)
public static PlateChamferBuilder.AngleMethod valueOf(String name)
public static PlateChamferBuilder.AngleMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.