public static class PillarBuilder.EndCutTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
No end cuts are applied
|
static int |
_SYMMETRIC
The same end cut is applied to both ends
|
static int |
_TWO_SIDED
Each end has different end cuts
|
static PillarBuilder.EndCutTypes |
NONE
No end cuts are applied
|
static PillarBuilder.EndCutTypes |
SYMMETRIC
The same end cut is applied to both ends
|
static PillarBuilder.EndCutTypes |
TWO_SIDED
Each end has different end cuts
|
Modifier and Type | Method and Description |
---|---|
static PillarBuilder.EndCutTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PillarBuilder.EndCutTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PillarBuilder.EndCutTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final PillarBuilder.EndCutTypes NONE
public static final PillarBuilder.EndCutTypes SYMMETRIC
public static final PillarBuilder.EndCutTypes TWO_SIDED
public static final int _NONE
public static final int _SYMMETRIC
public static final int _TWO_SIDED
public static PillarBuilder.EndCutTypes valueOf(int value)
public static PillarBuilder.EndCutTypes valueOf(String name)
public static PillarBuilder.EndCutTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.