public static class OrientationPointMethodsBuilder.PointMethodTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BY_DISTANCE
The boundary is defined by a distance from a reference object.
|
static int |
_BY_POINT
The boundary is defined by a location on the landing curve closest to a specified point.
|
static int |
_FROM_END
The boundary is defined by a distance from the end of the landing curve.
|
static int |
_FROM_START
The boundary is defined by a distance from the start of the landing curve.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
BY_DISTANCE
The boundary is defined by a distance from a reference object.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
BY_POINT
The boundary is defined by a location on the landing curve closest to a specified point.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
FROM_END
The boundary is defined by a distance from the end of the landing curve.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
FROM_START
The boundary is defined by a distance from the start of the landing curve.
|
Modifier and Type | Method and Description |
---|---|
static OrientationPointMethodsBuilder.PointMethodTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationPointMethodsBuilder.PointMethodTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final OrientationPointMethodsBuilder.PointMethodTypes BY_POINT
public static final OrientationPointMethodsBuilder.PointMethodTypes BY_DISTANCE
public static final OrientationPointMethodsBuilder.PointMethodTypes FROM_START
public static final OrientationPointMethodsBuilder.PointMethodTypes FROM_END
public static final int _BY_POINT
public static final int _BY_DISTANCE
public static final int _FROM_START
public static final int _FROM_END
public static OrientationPointMethodsBuilder.PointMethodTypes valueOf(int value)
public static OrientationPointMethodsBuilder.PointMethodTypes valueOf(String name)
public static OrientationPointMethodsBuilder.PointMethodTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.