public static class ExcessMaterialBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXCESS_MATERIAL
excess material placement method
|
static int |
_FIT_UP
fit up placement method (added in NX902)
|
static ExcessMaterialBuilder.Types |
EXCESS_MATERIAL
excess material placement method
|
static ExcessMaterialBuilder.Types |
FIT_UP
fit up placement method (added in NX902)
|
Modifier and Type | Method and Description |
---|---|
static ExcessMaterialBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcessMaterialBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcessMaterialBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExcessMaterialBuilder.Types EXCESS_MATERIAL
public static final ExcessMaterialBuilder.Types FIT_UP
public static final int _EXCESS_MATERIAL
public static final int _FIT_UP
public static ExcessMaterialBuilder.Types valueOf(int value)
public static ExcessMaterialBuilder.Types valueOf(String name)
public static ExcessMaterialBuilder.Types[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.