public static class CornerCutBuilder.CutOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CORNER
Create corner cut on selected corner point.
|
static int |
_PLATE
Create corner cut for all corner points of the mold face of plate body
|
static CornerCutBuilder.CutOption |
CORNER
Create corner cut on selected corner point.
|
static CornerCutBuilder.CutOption |
PLATE
Create corner cut for all corner points of the mold face of plate body
|
Modifier and Type | Method and Description |
---|---|
static CornerCutBuilder.CutOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerCutBuilder.CutOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerCutBuilder.CutOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final CornerCutBuilder.CutOption CORNER
public static final CornerCutBuilder.CutOption PLATE
public static final int _CORNER
public static final int _PLATE
public static CornerCutBuilder.CutOption valueOf(int value)
public static CornerCutBuilder.CutOption valueOf(String name)
public static CornerCutBuilder.CutOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.