public static class BracketBuilder.AlignmentTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTO_ALIGNMENT
The bracket molding faces is aligned to stiffener molding face
|
static int |
_DATUM_PLANE_ALIGNMENT
The bracket molding face is aligned to a datum plane
|
static BracketBuilder.AlignmentTypes |
AUTO_ALIGNMENT
The bracket molding faces is aligned to stiffener molding face
|
static BracketBuilder.AlignmentTypes |
DATUM_PLANE_ALIGNMENT
The bracket molding face is aligned to a datum plane
|
Modifier and Type | Method and Description |
---|---|
static BracketBuilder.AlignmentTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BracketBuilder.AlignmentTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BracketBuilder.AlignmentTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BracketBuilder.AlignmentTypes DATUM_PLANE_ALIGNMENT
public static final BracketBuilder.AlignmentTypes AUTO_ALIGNMENT
public static final int _DATUM_PLANE_ALIGNMENT
public static final int _AUTO_ALIGNMENT
public static BracketBuilder.AlignmentTypes valueOf(int value)
public static BracketBuilder.AlignmentTypes valueOf(String name)
public static BracketBuilder.AlignmentTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.