public static class ThreeBendCornerBuilder.OriginTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BEND_CENTER
The relief origin will be at the intersection of first bend's centerline and bisector of corner angle.
|
static int |
_CORNER_POINT
The relief origin will be at the corner point.
|
static ThreeBendCornerBuilder.OriginTypes |
BEND_CENTER
The relief origin will be at the intersection of first bend's centerline and bisector of corner angle.
|
static ThreeBendCornerBuilder.OriginTypes |
CORNER_POINT
The relief origin will be at the corner point.
|
Modifier and Type | Method and Description |
---|---|
static ThreeBendCornerBuilder.OriginTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThreeBendCornerBuilder.OriginTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThreeBendCornerBuilder.OriginTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ThreeBendCornerBuilder.OriginTypes BEND_CENTER
public static final ThreeBendCornerBuilder.OriginTypes CORNER_POINT
public static final int _BEND_CENTER
public static final int _CORNER_POINT
public static ThreeBendCornerBuilder.OriginTypes valueOf(int value)
public static ThreeBendCornerBuilder.OriginTypes valueOf(String name)
public static ThreeBendCornerBuilder.OriginTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.