public static class SMBoundaryConditionBuilder.ConstraintTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CURVE_ALONG_CURVE |
static int |
_CURVE_TO_CURVE |
static int |
_POINT_ALONG_CURVE |
static int |
_POINT_TO_POINT |
static SMBoundaryConditionBuilder.ConstraintTypes |
CURVE_ALONG_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
CURVE_TO_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
POINT_ALONG_CURVE |
static SMBoundaryConditionBuilder.ConstraintTypes |
POINT_TO_POINT |
Modifier and Type | Method and Description |
---|---|
static SMBoundaryConditionBuilder.ConstraintTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SMBoundaryConditionBuilder.ConstraintTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SMBoundaryConditionBuilder.ConstraintTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final SMBoundaryConditionBuilder.ConstraintTypes POINT_TO_POINT
public static final SMBoundaryConditionBuilder.ConstraintTypes POINT_ALONG_CURVE
public static final SMBoundaryConditionBuilder.ConstraintTypes CURVE_TO_CURVE
public static final SMBoundaryConditionBuilder.ConstraintTypes CURVE_ALONG_CURVE
public static final int _POINT_TO_POINT
public static final int _POINT_ALONG_CURVE
public static final int _CURVE_TO_CURVE
public static final int _CURVE_ALONG_CURVE
public static SMBoundaryConditionBuilder.ConstraintTypes valueOf(int value)
public static SMBoundaryConditionBuilder.ConstraintTypes valueOf(String name)
public static SMBoundaryConditionBuilder.ConstraintTypes[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.