public static class MiterOptions.PositionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BOTH
miter is done both at beginning and ending
|
static int |
_END
miter is done at the ending
|
static int |
_NONE
no miter
|
static int |
_START
miter is done at the beginning
|
static MiterOptions.PositionOptions |
BOTH
miter is done both at beginning and ending
|
static MiterOptions.PositionOptions |
END
miter is done at the ending
|
static MiterOptions.PositionOptions |
NONE
no miter
|
static MiterOptions.PositionOptions |
START
miter is done at the beginning
|
Modifier and Type | Method and Description |
---|---|
static MiterOptions.PositionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MiterOptions.PositionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MiterOptions.PositionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final MiterOptions.PositionOptions NONE
public static final MiterOptions.PositionOptions START
public static final MiterOptions.PositionOptions END
public static final MiterOptions.PositionOptions BOTH
public static final int _NONE
public static final int _START
public static final int _END
public static final int _BOTH
public static MiterOptions.PositionOptions valueOf(int value)
public static MiterOptions.PositionOptions valueOf(String name)
public static MiterOptions.PositionOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.