public static class FlexibleCableBuilder.BendAngleDirectionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMAL_DIRECTION
Bend angle normal direction.
|
static int |
_REVERSE_NORMAL_DIRECTION
Bend angle reverse normal direction.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
NORMAL_DIRECTION
Bend angle normal direction.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
REVERSE_NORMAL_DIRECTION
Bend angle reverse normal direction.
|
Modifier and Type | Method and Description |
---|---|
static FlexibleCableBuilder.BendAngleDirectionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexibleCableBuilder.BendAngleDirectionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexibleCableBuilder.BendAngleDirectionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlexibleCableBuilder.BendAngleDirectionOptions REVERSE_NORMAL_DIRECTION
public static final FlexibleCableBuilder.BendAngleDirectionOptions NORMAL_DIRECTION
public static final int _REVERSE_NORMAL_DIRECTION
public static final int _NORMAL_DIRECTION
public static FlexibleCableBuilder.BendAngleDirectionOptions valueOf(int value)
public static FlexibleCableBuilder.BendAngleDirectionOptions valueOf(String name)
public static FlexibleCableBuilder.BendAngleDirectionOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.