public static class FlangeBuilder.MatchFaceOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
The flange is placed on the selected edge
|
static int |
_UNTIL_SELECTED
The flange face is extended until the selected plane
|
static FlangeBuilder.MatchFaceOptions |
NONE
The flange is placed on the selected edge
|
static FlangeBuilder.MatchFaceOptions |
UNTIL_SELECTED
The flange face is extended until the selected plane
|
Modifier and Type | Method and Description |
---|---|
static FlangeBuilder.MatchFaceOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.MatchFaceOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.MatchFaceOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FlangeBuilder.MatchFaceOptions NONE
public static final FlangeBuilder.MatchFaceOptions UNTIL_SELECTED
public static final int _NONE
public static final int _UNTIL_SELECTED
public static FlangeBuilder.MatchFaceOptions valueOf(int value)
public static FlangeBuilder.MatchFaceOptions valueOf(String name)
public static FlangeBuilder.MatchFaceOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.