public static class DrawnCutoutBuilder.SectionSideOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LEFT
Side pointed to by the inverse of the tangent cross normal vector
|
static int |
_RIGHT
Side pointed to by the tangent cross normal vector
|
static DrawnCutoutBuilder.SectionSideOptions |
LEFT
Side pointed to by the inverse of the tangent cross normal vector
|
static DrawnCutoutBuilder.SectionSideOptions |
RIGHT
Side pointed to by the tangent cross normal vector
|
Modifier and Type | Method and Description |
---|---|
static DrawnCutoutBuilder.SectionSideOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawnCutoutBuilder.SectionSideOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawnCutoutBuilder.SectionSideOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawnCutoutBuilder.SectionSideOptions LEFT
public static final DrawnCutoutBuilder.SectionSideOptions RIGHT
public static final int _LEFT
public static final int _RIGHT
public static DrawnCutoutBuilder.SectionSideOptions valueOf(int value)
public static DrawnCutoutBuilder.SectionSideOptions valueOf(String name)
public static DrawnCutoutBuilder.SectionSideOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.