public static class BendBuilder.BendLocationOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CENTER_LINE |
static int |
_INNER_MOLD_LINE |
static int |
_MATERIAL_INSIDE |
static int |
_MATERIAL_OUTSIDE |
static int |
_OUTER_MOLD_LINE |
static BendBuilder.BendLocationOptions |
CENTER_LINE |
static BendBuilder.BendLocationOptions |
INNER_MOLD_LINE |
static BendBuilder.BendLocationOptions |
MATERIAL_INSIDE |
static BendBuilder.BendLocationOptions |
MATERIAL_OUTSIDE |
static BendBuilder.BendLocationOptions |
OUTER_MOLD_LINE |
Modifier and Type | Method and Description |
---|---|
static BendBuilder.BendLocationOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendBuilder.BendLocationOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendBuilder.BendLocationOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BendBuilder.BendLocationOptions OUTER_MOLD_LINE
public static final BendBuilder.BendLocationOptions CENTER_LINE
public static final BendBuilder.BendLocationOptions INNER_MOLD_LINE
public static final BendBuilder.BendLocationOptions MATERIAL_INSIDE
public static final BendBuilder.BendLocationOptions MATERIAL_OUTSIDE
public static final int _OUTER_MOLD_LINE
public static final int _CENTER_LINE
public static final int _INNER_MOLD_LINE
public static final int _MATERIAL_INSIDE
public static final int _MATERIAL_OUTSIDE
public static BendBuilder.BendLocationOptions valueOf(int value)
public static BendBuilder.BendLocationOptions valueOf(String name)
public static BendBuilder.BendLocationOptions[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.